ADG1636 Suitability

I am looking for analog switches.

The first is SPDT two channel. It must be capable of switching between a 0 to 14v square wave signal and a -5 to +14v zero crossing square wave  signal. Current less then 10mA

The second is SPDT two channel. It must be capable of switching high and low. The high voltage is 14 volts. Low is 0 volts. Current 100 mA.or more.

I have found the ADG1636.  Is this suitable for both. If not, what do  recommend.

Ray.