Post Go back to editing

ADG508F ESD rating

Thread Summary

The user inquired about the ESD tolerance of the ADG508F analog inputs and the internal ESD diode architecture. The final answer confirmed that the ADG508F can withstand ±300 V HBM ESD without dedicated protection. The engineer suggested considering the ADG5208F or ADG5248F for higher ESD ratings (4kV HBM).
AI Generated Content

I use an ADG508F.

Q1)How much ESD can the ADG508F(Analog input from S1 to S8) take?

(It is not written in the datasheet.)

Q2)Can you provide the  internal ESD diode architectures?

(Diode Stacks or Back to Back Diodes ?)

already seeing below Analog Dialogue. (fig4,5 OP-AMP ESD architectures) 

Regards,

 

http://www.analog.com/en/analog-dialogue/articles/esd-diodes-as-voltage-clamps.html