Post Go back to editing

Looking for AD chip, the same as FST3125MX

Thread Summary

The user seeks a 4-key AD chip with parameters superior to the ADG774BRQZ, specifically low Ron (<2 ohms) and a switching frequency below 120 MHz. The final answer recommends the ADG712 or ADG812, both 4 x SPST switches, with the ADG812 offering the lowest Ron and the ADG712 providing a larger signal bandwidth.
AI Generated Content

Hello! I'm looking for AD chip that would be on the keys and management would like FST3125MX, but in the parameters better than ADG774BRQZ

That is, I'm looking for a chip AD, which would be 4 keys (no longer necessary). These keys must be controlled by separate signals. The resistance in the open state is less than 2 oHms. Low level control - the keys are open, a high level of control - the keys are closed. The switching frequency of the keys below 120Mhz.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.