Post Go back to editing

Off State Leakage of ADG201A-EP

I know from datasheet of ADG201A-EP that the maximum OFF state leakage of this IC with power supply =+/-15V and VD = ±14 V, VS = ∓14 V is 100nA. This leakage is too much for the circuit that I am designing. But the input signal range in my application is much less that that is given in the datasheet. Power supply to this IC is +/-15V. The input signal range will be +/- 2V. I would like to know what will be the maximum OFF state leakage for this IC over the operating temperature range of -55C to 125C for this input range? Will there be a reduction from the datasheet values?

Thanks

Shihab.

Parents
  • Hi Shihab,

    I can now understand the problem.

    On the SPICE model, please put an asterisk sign (*) before RC1, RC2, and RC3. 

    These resistors are the one causing the leakage.

    Thank you for bringing this to our attention. We shall update the existing SPICE model.

    Best Regards,

    May

Reply
  • Hi Shihab,

    I can now understand the problem.

    On the SPICE model, please put an asterisk sign (*) before RC1, RC2, and RC3. 

    These resistors are the one causing the leakage.

    Thank you for bringing this to our attention. We shall update the existing SPICE model.

    Best Regards,

    May

Children
No Data