Post Go back to editing

Off State Leakage of ADG201A-EP

I know from datasheet of ADG201A-EP that the maximum OFF state leakage of this IC with power supply =+/-15V and VD = ±14 V, VS = ∓14 V is 100nA. This leakage is too much for the circuit that I am designing. But the input signal range in my application is much less that that is given in the datasheet. Power supply to this IC is +/-15V. The input signal range will be +/- 2V. I would like to know what will be the maximum OFF state leakage for this IC over the operating temperature range of -55C to 125C for this input range? Will there be a reduction from the datasheet values?

Thanks

Shihab.

Parents
  • Hi David,

    Thank you for the reply. Sorry for the mistake in the schematic. There should be 10kohm between P5V & D1 and N5V & S1. In this circuit I was expecting 0V across R1 but I am getting 186.8mV. Can you please explain the reason? Is it an IC spice model issue or is the simulation result I am getting is as per design?

    Thanks,

    Shihab.

Reply
  • Hi David,

    Thank you for the reply. Sorry for the mistake in the schematic. There should be 10kohm between P5V & D1 and N5V & S1. In this circuit I was expecting 0V across R1 but I am getting 186.8mV. Can you please explain the reason? Is it an IC spice model issue or is the simulation result I am getting is as per design?

    Thanks,

    Shihab.

Children
No Data