Post Go back to editing

ADG749: SPICE Noise Analysis

Thread Summary

The user is experiencing high noise levels in LTSpice simulations involving the ADG749 switch, with the integrated RMS voltage noise from 1 Hz to 100 MHz being about 540 µV, much higher than the theoretical 4.26 µV. The final answer confirms that the ADG749 spice model does not include noise parameters. The user is advised to consider using the ADG714 EVAL-6SC70EBZ evaluation board for noise analysis or to model the ADG749 using its typical ON resistance and capacitances.
AI Generated Content

Hi,

I'm perfoming a noise analysis in LTSpice. My circuit includes the ADG749, therefore I downloded the provided Spice model (.cir), and created an appropriate symbol in LTSpice (which I have already done several times).

By performing my noise analysis in LTSpice, the results are "terrible" large. It seems, the used switch (ADG749) causes the additional noise. 

I attached the simulation result obtained in LTSpice for a single switch. The integrated RMS voltage noise from 1 Hz to 100 MHz is about 540µV. As can be seen, Rin and R1 are noiseless, so the whole noise is added by the switch. Comparing this result with my theoretical resullt of v_n = sqrt(4 x k x R x T x B * pi/2) = 4.26 µV (k = Boltzmann constant; R = 7 Ohm, worst case value according to the datasheet; T = 300 °K; B = 100 MHz), the simulatuion result is way to large.

I had a lock in the .cir file. I wasn't able to identify any noise-values. So I think the switch doesn't include a noise model. But I'm still curiose why the switch has this strange noise behaviour.

Has anyone experience with noise simulations including switch models?

BR

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.