Post Go back to editing

TG07 SUFFIX MEANING FOR CUSTOMER HONEYWELL REQUIREMENT

Thread Summary

The user inquires about the meaning of the 'TG07' suffix for the MAX306EQI-TG07 device, suspecting it indicates a customer-specific variant. The final answer confirms the suffix and requests clarification on whether it is 'TG07' or 'TG070'. Additional context indicates that the device is a lead finish and not RoHS compliant, with a date code of 0446.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX306EQI-TG07

MAX306EQI-TG07 is device Rochester has on hand from Analog Devices.  There are no records showing the meaning of TG07, which nomenclature for Maxim shows customer special. Is there any change to form, fit or function? This is lead finish device and not RoHS correct?  Date Code 0446.  Please advise either of document or statement can advise customer.  Need as soon as possible. 

Thank you,

Vicki Shigley

vshigley@rocelec.com 

480-674-8179

Parents Reply Children
No Data