MAX14662
Production
The MAX14662 is a serially controlled 8 x SPST switch for general purpose signal switching applications. The number of switches makes the device useful...
Datasheet
MAX14662 on Analog.com
Hello,
We are using two MAX14662 devices in SPI daisy-chain mode to multiplex external sensor power channels. See below schematics. We shift a 16-bit word every 10 ms so that only one switch channel should be closed at a time. Nothing is currently connected at the outputs.
We observe an intermittent issue on the second MAX14662, channel B7. When turning ON U23.B1 and turning OFF U24.B7, U23.B1 updates immediately at the CS rising edge, but U24.B7 sometimes remains on for approximately 2 ms before turning off. This creates a temporary overlap where both channels are on.

Below capture shows U24.B7 first turning OFF at the same time as U23.B1 is being turned ON. Next cycle it turns OFF approximately 2 ms too late.

Channel 1-4 is SPI communication
Channel 0 = U23.B1
Channel 7 = U24.B7
Things we have verified:
According to the datasheet, switches should update on the rising edge of CS, and tOFF is specified in the microsecond range. We would therefore not expect a millisecond-scale delayed turn-off after a valid SPI frame.
Questions:
Best regards
/F