MAX322
Production
The MAX320/MAX321/MAX322 are precision, dual, SPST analog switches designed to operate from ±3V to ±8V dual supplies. The MAX320 has two normally open...
Datasheet
MAX322 on Analog.com
Hello all,
I was unable to find any information regarding marking (or its format) in regard to MAX3221CAE+T in datasheet.
per customer concern, I would need an official source to confirm so if possible
Any help or directions are appreciated, thanks.