Hi
I have made schematics for I2C Controlled 4 x 4 USB matrix using 8 x MAX4899AEETE+T 4 x MAX7310 and 1 x ADG2188.
Could you please help me with setting the default address for ADG2188.
Also see if I have missed any supporting components needed for the Ic’s to work?
Am I reading the datasheets correctly that the reset pins for ADG2188 and MAX7310 should be pulled high through 10k resister then shorted to ground to rest them?
Below are the 2-part schematics.
Thanks
MSC2000