Post Go back to editing

I2C Controlled 4 x 4 USB matrix using 8 x MAX4899AEETE+T 4 x MAX7310 and 1 x ADG2188

Thread Summary

The user asked for help setting the default I2C address for the ADG2188 and ensuring the correct reset configuration for the ADG2188 and MAX7310 in a USB matrix design. The engineer confirmed that the ADG2188 address is set by A2, A1, and A0, and advised pulling the RESET pins high through 10kΩ resistors and momentarily shorting to ground for reset. The user updated the design, setting AD0 high on the second ADG2188 to change its address to 1110001.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX4899AE

Hi

I have made schematics for I2C Controlled 4 x 4 USB matrix using 8 x MAX4899AEETE+T 4 x MAX7310 and 1 x ADG2188.

Could you please help me with setting the default address for ADG2188.

Also see if I have missed any supporting components needed for the Ic’s to work?

Am I reading the datasheets correctly that the reset pins for ADG2188 and MAX7310 should be pulled high through 10k resister then shorted to ground to rest them?

Below are the 2-part schematics.

Thanks

MSC2000

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.