Hi,
I am designing an analog RGB matrix switch.
Can I connect the AVEE terminal to AGND with the AD8108/AD8109 as a single power supply amplifier?
Because of the analog RGB voltage range is 0 to 0.7 V.
AD8109
Production
The AD8108/AD8109 are high speed 8 × 8 video crosspoint
switch matrices. They offer a −3 dB signal bandwidth greater than
250 MHz and channel switch...
Datasheet
AD8109 on Analog.com
AD8108
Production
The AD8108/AD8109 are high speed 8 × 8 video crosspoint
switch matrices. They offer a −3 dB signal bandwidth greater than
250 MHz and channel switch...
Datasheet
AD8108 on Analog.com
Hi,
I am designing an analog RGB matrix switch.
Can I connect the AVEE terminal to AGND with the AD8108/AD8109 as a single power supply amplifier?
Because of the analog RGB voltage range is 0 to 0.7 V.
PoornimaSubramani - Moved from Video to Switches/Multiplexers. Post date updated from Monday, April 28, 2025 2:35 AM UTC to Monday, April 28, 2025 7:49 AM UTC to reflect the move.
Hi Taksh, Gauzz will help out here.
Hi,
At single supply the input signal you have mentioned won't be recognized by the part as the input voltage range is limited to these values.![]()
These were specified at +/- 5V.
Regards,
Goz
Hi Gauzz, Thanks for your reply.
I use this IC with +/- 5V.
Best Regards,