1. How much current does SDI consume when communicating?
2. How much is the internal pull-up resistance of SDO in ADGS1414D?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADGS1414D
Recommended for New Designs
The ADGS1414D contains eight independent SPST switches. A serial peripheral interface (SPI) controls the switches. The SPI has robust error detection features...
Datasheet
ADGS1414D on Analog.com
1. How much current does SDI consume when communicating?
2. How much is the internal pull-up resistance of SDO in ADGS1414D?
Hi,
The internal pull-up resistor is a 1k Ohm resistor.
For how much current SDI consumes, please refer to the Power Requirements section of the spec tables.
Regards,
Karen
Thank you for your answer!
I have a more question
1. If the SDI draws around 1 mA of current, the voltage becomes 3.3 V – 1.25 V = 2.05 V. Should I understand this 2.05 V as the minimum voltage? (Please refer to the table below.)

2. If the above description is correct, in the case of ADGS1414D, when connected by Daisy chain, SDI acts as SDO's source current, so SDO can't come out 3.3V, is it correct?
Hi,
The SDI should never draw 1mA of current, see spec table below.

Here are some scope plots of the ADGS1414D whilst in Daisy Chain mode with SCLK @ 2.5 MHz. Vdd = +15V, Vss = -15V, and Vs = +10V. Temp = 25C.
As you can see SDI of unit one is 3.3V, so is SDO of unit 1 and SDO of unit 2.
SPI Mode 0, VL=3.3V :

SPI Mode 3, VL=3.3V :

Regards,
Karen
Thank you for your answer!
I have more question.
Can I ask questions in the comments here, or should I create a new post?
If it's still relating to the ADGS1414D, you may ask it here.
This is the result of measuring the SDO waveform of the 3rd ADGS1414D by SPI frequency by connecting 3 ADGS1414D by Daisy chain.
1. 2.5MHZ (As measured by the head office, SDO output is measured at 3.2V.)

2. 5MHZ (The SDO output is at 3.2V, but the waveform at Rising starts to lie down.)

3. 12.5MHZ (The SDO output is 2.68V, and the load current increases as the frequency increases, causing the waveform to lie down more and fail to rise to 3.2V.)

4. 25MHZ (The SDO output is 1.92V, and as the frequency increases, the load current increases further, resulting in a lower voltage output.)

The part where the load current increases for each frequency is shown in Datasheet, so I understand, but the problem is that the waveform is lying down too much compared to the increasing load current.

25 MHz based on Datasheet, 120uAtyp for SDI based on VL = 3.3V.
Currently, we proceed with control with FPGA, and the current allowable current per IO is 16mA.
When three ADGS1414D are connected by Daisy chain, the current capacity of FPGA IO is sufficient even if it is operated at 25 MHz, which is a separate issue from FPGA IO strength, and the load current capacity of 1A is sufficiently being tested for VL voltage.
Can you check the SDO waveform at 25 MHz?
If you get the same result as us, please check what the cause is and if there is a solution,
If there is a 3.3V output, which is a different result, I would like you to comment on which part we should change additionally.
Judging from your scope plots here, it looks like you are having an issue with capacitance, which is something that doesn't appear delay the system at 2.5MHz enough to read the SDO at any lower than 3.2V, but is certainly is adding a slow rise on the rising edge.
I would suggest checking your circuit / board. Are there any parasitic capacitances connected in between your two ADGS1414Ds?
From the datasheet below, t8, t9, t10, and load cap below should be satisfied if SDO will be used.


We have reviewed based on your reply. However, we have ADGS1414D connected on the 1st floor of PCB and the connected distance is also very short. Therefore, I think the impact of the capacitance you mentioned is limited.
Can you measure the SDO waveform in 2.5 MHz, 12.5 MHz, and 25 MHz in Daisy chain mode? and
Can you give me an artwork guide?
We have reviewed based on your reply. However, we have ADGS1414D connected on the 1st floor of PCB and the connected distance is also very short. Therefore, I think the impact of the capacitance you mentioned is limited.
Can you measure the SDO waveform in 2.5 MHz, 12.5 MHz, and 25 MHz in Daisy chain mode? and
Can you give me an artwork guide?