MAX14763
Production
The MAX14759/MAX14761/MAX14763 analog switches are capable of passing bipolar signals that are beyond their supply rails. These devices operate from a...
Datasheet
MAX14763 on Analog.com
MAX14673
Production
The MAX14670–MAX14673 provide protection to valuable consumer circuits against positive voltage faults up to +28VDC. An internal clamp also protects the...
Datasheet
MAX14673 on Analog.com
Hello,
What is the maximum toggle frequency achievable on SEL pin of MAX14763?
I would like to switch between A1 and A2 in few hundred kHz range.
Hi hunl ,
Thanks for clarifying. The datasheet for the MAX14763 does not specify the maximum toggle frequency for the SEL pin.
However, similar devices typically support toggle frequencies up to a few hundred kHz sometimes up to 1 MHz.
We can test this on our end, but we also need to know your application and the signal frequency you plan to use on the SEL pin.
Regards,
Gelo
Hi hunl ,
Thanks for clarifying. The datasheet for the MAX14763 does not specify the maximum toggle frequency for the SEL pin.
However, similar devices typically support toggle frequencies up to a few hundred kHz sometimes up to 1 MHz.
We can test this on our end, but we also need to know your application and the signal frequency you plan to use on the SEL pin.
Regards,
Gelo