ADG726
Production
The ADG726/ADG732 are monolithic, complementary metal oxide semiconductor (CMOS) 32-channel and dual 16-channel analog multiplexers. The ADG732 switches...
Datasheet
ADG726 on Analog.com
I want to use ADG726 for IO mux. I want to connect VDD=5V. Can you give me supply dissipation or required maximum supply current of ADG726?
Hi OzanGuney ,
The ADG726 typically has a supply current (Idd) of 10 µA. At a supply voltage (Vdd) of 5 V, the power dissipation is approximately 50 µW. The maximum continuous current per channel is 30 mA.
Best regards,
Christian
I see. I will choose a supply converter that give >50uW. Maybe 100-200uW. Is it true?