Hello,
I have a quick question on the logic inputs of the MAX4784EUE+. Can digital signals with High-Signal at 3.3V (at which level my microcontroller supplies) be used as logic signals? Thanks a lot!
Best greetings
MAX4784
Production
The MAX4780/MAX4784 are low on-resistance, low-voltage, quad 2:1 analog multiplexers that operate from a single +1.6V to +4.2V supply. These devices have...
Datasheet
MAX4784 on Analog.com
Hello,
I have a quick question on the logic inputs of the MAX4784EUE+. Can digital signals with High-Signal at 3.3V (at which level my microcontroller supplies) be used as logic signals? Thanks a lot!
Best greetings