Post Go back to editing

About JP1 and 2 settings of EVAL-ADGS1414D

Category: Hardware
Product Number: ADGS1414D

Hi

I'm concidering ADGS1414D.

Now I have a question.

For EVAL-ADGS1414D, you can set whether to use an SDP board or an external connection by setting JP1 and 2.


However, the setting conditions in Table 2 and the circuit diagram in Figure.9 seem to be opposite.
Which is the correct connection?

Best regards,

Yuya

Parents Reply
  • Hi, Karen

    Thank you for your answer.

    In that case, the description in Table 1 and "When using the SDP-B controller board in conjunction with the EV-ADGS1414DSDZ, place JP1 in Position B to avoid damage to the SDP-B." is also reversed, right?

    After setting the ADGS1414D switch, I would like to remove the SDP board while maintaining the switch settings.

    Best regards,

    Yuya

Children