Post Go back to editing

About JP1 and 2 settings of EVAL-ADGS1414D

Category: Hardware
Product Number: ADGS1414D

Hi

I'm concidering ADGS1414D.

Now I have a question.

For EVAL-ADGS1414D, you can set whether to use an SDP board or an external connection by setting JP1 and 2.


However, the setting conditions in Table 2 and the circuit diagram in Figure.9 seem to be opposite.
Which is the correct connection?

Best regards,

Yuya

Parents Reply Children
  • Hi, Karen

    Thank you for your answer.

    In that case, the description in Table 1 and "When using the SDP-B controller board in conjunction with the EV-ADGS1414DSDZ, place JP1 in Position B to avoid damage to the SDP-B." is also reversed, right?

    After setting the ADGS1414D switch, I would like to remove the SDP board while maintaining the switch settings.

    Best regards,

    Yuya

  • Hi Yuya,

    Unfortunately, yes, this is a continuous typo throughout this user guide.

    After setting the ADGS1414D switch, removing the SDP board resets the device.

    Regards,

    Karen 

  • Hi, Karen

    When I checked the evaluation board, I think the mistake was in the wrong place.

    Isn't A and B in Figure 9 opposite and Table 2 correct?
    (Confirmed with a tester)

    If I just set JP1 to Position A and supply VL externally, can I safely remove the SDP board without damaging the SDP board after setting the switch?

    Best regards,

    Yuya

  • Hi Yuya,

    In the newest released versions of the board, this has been corrected and pins A & B correspond to Table 2.