Post Go back to editing

Alternatives to ADGS2414D for switching by I2C

Thread Summary

The user is seeking an I2C-controlled switch IC capable of handling at least 100 mA per channel for a potentiostat design. The MAX14724 was suggested, but it only supports 50 mA per pin. The MAX14662 was also recommended as a potential solution.
AI Generated Content
Category: Hardware
Product Number: ADGS2414D

Hi, I am working on a potentiostat in which the OPAMP must provide a selectable feedback resistor (so I thought of a controlled switch/mux), with a maximum continuous flowing current of 100 mA. The entire board has I2C devices working at 400 kHz (no SMBus then). I noticed that a new integrated circuit (the ADGS2414D) is now available that would be suitable for my design, but only works with SPI interface. I also foudn the ADG729 but only supports at maximum 30 mA per channel. I was wondering if something similar exists but controlled through I2C interface instead of SPI. The IC must provide at least 4 switches (8 is better), I2C controlled, capable of supporting at least 100 mA per channel. I can't find it in the AD products catalogue, is there any filter to be applied to ease the research for I2C devices? 

Thank you for your support.

Mattia

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.