Post Go back to editing

Analogue power supply lower limits

Category: Hardware
Product Number: AD75019

Dear All,

I have some question about the power supply requirements of the AD75019. From the datasheet, the "Voltage Range, Total Analog" minimum value is 9V. I would like to supply the analogue part between 0V (the VSS) and 1.5V (the VDD), which is obviously lower than the suggested value. However I am now trying to supply between 0V (the VSS) and 5V the (VDD) and it seems working. Are there some tests you suggest to do to check if everything is working properly? The reason I want to keep the voltage as much as possible low is because they will be connected to custom devices fabricated in our lab and I would like to keep the voltage as low as possible (my devices are working between 0V and 1.2V).

In case I would like to supply with even less voltage, like 3.3V or 1.5V, is there something I can do to check if everything is working properly?

Thank a lot,

Saverio