Post Go back to editing

Can unsued ports (inputs and outputs be left floating)?

Thread Summary

The user inquires about leaving unused ports (S3A/B, S4A/B, D3, D4, IN3, IN4) of ADG1634 ICs floating. The final answer recommends connecting S3A/B and S4A/B to GND via resistors, and D3 and D4 can be left floating or connected to GND via resistors. IN3 and IN4 can float. The accompanying answer clarifies that connecting S3 and S4 to GND via resistors is not mandatory but recommended.
AI Generated Content
Category: Hardware
Product Number: ADG1634

Hello,

I am using several ADG1634 ICs in my board but in the last one, I only use two ports (S1A/B & D1 and S2A/B & D2). S3/D3 and S4/D4 are unused at all.

Is it okay if I leave the S3A/B, S4A/B, D3 and D4 floating? What about IN3 and IN4?

Thank you.

Parents Reply Children
No Data