Post Go back to editing

DG301 supply current

Thread Summary

The user inquired about the negative supply current of the DG301ACWE+ at different VIN levels. The support engineer confirmed that the current is -100uA at VIN = 0.8V and -100mA at VIN = 4V, noting these values are correct and reflect the switch's state. The user acknowledged the higher current consumption when the switch is on. The engineer suggested considering newer switch models for potentially better performance.
AI Generated Content
Category: Hardware
Product Number: DG301ACWE+

Hi

I’m considering DG301ACWE+.

Now I have a question.

This is about electrical characteristics (Over Temperature).

Looking at negative supply current.
When VIN = 0.8V, it is -100uA, but when VIN = 4V, it is -100mA.
Is this correct? Is it a typo?
Please tell me the exact current consumption.

Best regards,
Yuya