Post Go back to editing

High current switching

Category: Hardware

Hi,

I have an application that needs to switch multiple 9v loads at both anode and cathode ends. It is an array of 8 x 14 solenoids which run at 9v and about 100mA each. They need a pulse of about 150ms to operate. The 14 solenoids are arranged in pairs and only one of the pair will be activated at a time, so I need to switch the cathode end between each pair. At the anode end I need to route the 9v to one of the arrays at a time.

So I think I'm looking for something like the MAX4660 for the cathode end as it can handle 200 mA but I'd like a more convenient package with more than a single SPDT switch in it.

For the anode end I need an SPST equivalent and again would like all 8 in one package if possible but of course the total current will be multiplied by the number of internal switches.

Ideally control would be through a 3.3v GPIO line but I can live with SPI or I2C if I have to.

I hope that makes sense! I have looked through about a baziliion datasheets and can't find what I'm looking for so I was hoping someone with more experience would know?

Thanks in advance for your help.

cheers,

Adam

  • Hi AdamCSL,

    Great that you're looking at Analog Devices for this, but our product lineup in this category is limited. Under "Solenoid Drivers" there are a couple of devices that are more targeted at stepper motor applications:

    https://www.analog.com/en/product-category/solenoid-driver.html

    If those are overkill, the L293D from other manufacturers might be a simple solution. This chip is popular on Arduino and other maker-style motor driver boards.

    -Mark

  • Thanks for the response but it's not the kind of solenoid that needs a stepper motor. It's actually a mechanical 7 segment digit display and the solenoids turn each segment either yellow or black, depending which one of the pairs of cathodes you connect. A single timed pulse is all that's required so a fast switch is actually ideal.

    The L293D might be useful for a completely different project where I need to reverse the polarity instead of routing to a different cathode so thanks for that!

    cheers,

    Adam

  • Is something like the ULN2003 what you're after for driving the low sides of the coils? It's only 7 channels, but they're fairly inexpensive and you can probably find similar with 8. Again this isn't in ADI's product line, just giving some hints on where to look. For the high side drivers, you could implement this discretely - do a search on "high side coil driver" or "high side solenoid driver" and a bunch of circuits will pop up.

    And after another quick search, it does look like there are a few more options in ADI's lineup, but again, likely overkill: https://www.analog.com/en/product-category/dc-motor-driver.html 

    It sounds like you need independent control of high-side and low-side drivers, rather than half-bridge - which can be made to work by enabling one of the drivers or disabling  both, but there's probably a more elegant solution. 

    Also re: anode / cathode, I assume you're referring to a frewheeling diode wired in parallel to the solenoid? A napkin sketch of your circuit would help.

    -Mark

  • Hi Mark,

    Yes I'm currently using ULN2803 darlington array to test the devices and logic etc. but it doesn't solve the issue of switching between the yellow and black segments and if I have to add another component to do that I figured I could just replace the darlington with a SPDT switch and that would kill two birds with one stone. Here is the current test setup showing just the yellows and just one display. I could probably still use a darlington for the anode switching in the final circuit.

  • Gotcha - I guess the choice is yours - if you can find a PNP darlington and make an inverter out of an NPN to drive its base, that would work.

    The main apprehension with the MAX4660 is not exceeding abs max when the solenoids switch - the ULN2803 has internal clamp diodes, you'd want to add these externally when using the MAX4660. While the MAX4660 LOOKS like it has these diodes already - see datasheet Figure 1 and associated text - they are for ESD protection during handling, not intended for absorbing inductive "kick".

    -Mark

  • Thanks Mark... so something like this which would cover all 14 channels? It says it's primarily for ESD but also mentions clamping...

    uk.rs-online.com/.../1714298P

  • So the only answer I can give is to follow all datasheet abs max values verbatim. There is a note in the MAX4660 datasheet:

    Signals on NO, NC, COM, or INexceeding V+ or V- are clamped by internal diodes. Limit forward-diode current to maximum current rating.

    with currents listed in the tables. The Littlefuse clamp has a forward drop of:

    "The SCR structures are designed for fast triggering at a threshold of one +VBE diode threshold above V+ (Pin 16) or a -VBE diode threshold below V- (Pin 8)"

    This is about 0.7 V, so what this means is that the MAX4660 internal diode may end up absorbing all of the current, before the Littlefuse clamp turns on.

    In summary - it would be better to use external Schottky diode clamps, which have a lower forward drop. You may be able to find a Schottky diode array, similar to the Littlefuse part.

    -Mark

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.