Post Go back to editing

USB-SPI interface to use with ADGM1003 SP2T

Thread Summary

The user is looking for a USB to SPI interface/bridge to control an SP2T (ADGM1003) switch. The recommended solution is to use the SDP-B interface board and the ACE software, both of which are compatible with the ADGM1003 and can be used to control it via a PC USB port. The thread was moved to the switches/multiplexer forum for better visibility.
AI Generated Content
Category: Hardware
Product Number: ADGM1003

Hello, does anyone know of an ADI SMD component or other US based manufacturer of a USB to SPI interface/bridge that I can use to control an SP2T (ADGM1003) ?

Many Thanks!

BillU