Post Go back to editing

Self-Test when using AD598 with ADG858

Thread Summary

The user is experimenting with a project using the AD598 with an RDVT sensor and wants to perform a self-test during power-on. The final answer confirms that the ADG858 or ADG836 can be used to loop the excitation output (Exc 1 and Exc 2) to the AD598 inputs (Va and Vb) for the self-test, ensuring the output voltage is within the signal input range.
AI Generated Content
Category: Hardware

Hello and Greetings,

I'm experimenting with a project which uses AD598 with RDVT sensor.

The issue here is I need to make a self-test of the parts during power on.

And I've been wondering if I can use the Excitation (Exc 1 and Exc 2) direct to the AD598 inputs (Va and Vb) just to prompt the controller that the part (AD598 and/or ADG858) is OK and the signal path is OK.

And to do this, I've added ADG858 as an analog mux to set the default (connection to actual LVDT) or test mode (connection loop)

Best Regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.