Post Go back to editing

ADG1436 with LFCSP Package.

Thread Summary

The user asked about the correct temperature for installing a part with a heat gun, noting that 260°C, the maximum temperature for an SMT oven, was insufficient. The final answer suggested pre-heating the board and using flux, as 260°C should be sufficient for reflow. The user reported high impedance readings on pins 1-2 and 9-10 after rework, which the engineer confirmed as normal when the switch is not powered or the channel is not selected.
AI Generated Content
Category: Hardware
Product Number: ADG1436

Hi, I would like to know the temperature that should be used to install a part with a heat gun. 

The data sheet shows 260C using a SMT oven, but with a heat gun that temperature doesnt work,  it requires more but how much more before damaging the part?

Thank you 

Edit Notes

mobed and updated tags
[edited by: Sara Campbell at 6:11 PM (GMT -4) on 24 Jul 2023]
  • Hi AVESD,

    The 260 °C is already the maximum temperature. Beyond this may cause permanent damage to the device. This temperature should be enough to reflow the IC as you can see in the Figure 15 below. I got this figure on page 7 of AN-772 which is a guide for design and manufacturing of LFCSP. Have you tried pre-heating the board and adding flux during reflow? 

    Regards,

    Yoworex

  • Hi, and thank you for the quick response.

    As shown in the figure, I followed your advice and preheated the board. I preheated the board for about 4 minutes, and the reflow took about one minute, not exceeding 260C

    I noticed pins 1-2 and 9-10 are reading high impedance, something in the order of 5 to ~10 Mega ohms. The devices measure ∞ infinite resistance in pins 1-2 and 9-10 before the rework. The pads in the board also read infinite without components. I wonder if this is a normal condition for the device to read high impedance after the rework or if they are getting degraded.

    Please advise.

  • Hi AVESD,

    Pin 1 = D1, Pin 2 = S1B, pin 9 = D2, & Pin 10 = S2B. These pins should be high impedance when the switch is not powered, not enabled, or the channel is not selected. 

    Try the test setup below and see if there are abnormalities like drawing too much supply current, channel not switching, and etc. 

    Regards,

    Yoworex

  • Thanks a lot.

    I will give it a try. Just to make sure, if I probe pins 1 with pin 2 and pin 9 with pin 10 without any power it should read high impedance, correct?

  • Hi AVESD,

    Yes, you should see high impedance in those pins. In no power condition, the switch channels (SxA to D or SxB to Dx) should have high impedance. 

    Regards,

    Yoworex