Hi, I want to use ADG1222 for switching applicaton on my circuit. I have 3 question about ADG1222
1) I am only use first channel. I am not able to understand should I connect all other pins to ground except, Vdd, Vss, S1, D1, IN1.
2)I am also wondering which components or values should I use for bulk and bypass capacitors to input voltages ?
3) What are the effects of usage +-15V instead of using +-5V ?
Thanks for help in advance.
not in topic
[edited by: Erdogdu at 8:53 AM (GMT -4) on 20 Jul 2023]