What is the difference between MAX307CWI+ and DG407CWI+?
Or else could you suggest an alternate against MAX307CWI+ which have similar specification as well as active in status
MAX307
Production
The MAX306/MAX307 precision, monolithic, CMOS analog multiplexers (muxes) offer low on-resistance (less than 100Ω), which is matched to within 5Ω between...
Datasheet
MAX307 on Analog.com
DG407
Production
Maxim's redesigned DG406 and DG407 CMOS analog multiplexers now feature guaranteed matching between channels (8Ω max) and flatness over the specified...
Datasheet
DG407 on Analog.com
What is the difference between MAX307CWI+ and DG407CWI+?
Or else could you suggest an alternate against MAX307CWI+ which have similar specification as well as active in status
Hi Manojkumar888,
The MAX307 is the upgrade version of DG407 (better Ron matching, Ron flatness and lower leakage across temperature).
Or else could you suggest an alternate against MAX307CWI+ which have similar specification as well as active in statu
MAX307CWI+ is still active but if you need an alternative, please give more information about your application and key parameter.
Regards,
Yoworex