Post Go back to editing

ADG918 RF switch

Product Number: ADG918

I bought a ADG918 EVAL board. Here is the configuration: A modulated signal source 72Mhz sent into the RFC pin; 2.75V Vdd voltage; 1Mhz 0~1.5v square wave was in control pin.

Schematic:

Input on RFC pin: modulated 72Mhz

When power it on, the yellow is the output.

Q1: why there is a DC slop when it's off. I placed a capacitor before the input to isolate the DC voltage. 

Q2: Can the input sinwave becomes a +/- sin wave let's say -1.5v to 1.5v peak to peak?

Parents Reply Children