HI
I am DFAE in Japan.
Does ADG1419 work at VDD=19.5V and VSS=0V ?
Best regards
N.Kokubo
ADG1419
Production
The ADG1419 is a monolithic iCMOS® device containing a
single-pole/double-throw (SPDT) switch. An EN input on the
LFCSP is used to enable or disable the...
Datasheet
ADG1419 on Analog.com
HI
I am DFAE in Japan.
Does ADG1419 work at VDD=19.5V and VSS=0V ?
Best regards
N.Kokubo
Hi N.Kokubo,
Apology for the confusion. It is still within the absolute maximum range but it is only recommended in the spec table under single supply that VDD should have a minimum of 5V and a maximum of 16.5V.
You may consider ADG5419 as an alternate, as it can operate to 40V single supply.
Regards,
Yoworex
Hi N.Kokubo,
Apology for the confusion. It is still within the absolute maximum range but it is only recommended in the spec table under single supply that VDD should have a minimum of 5V and a maximum of 16.5V.
You may consider ADG5419 as an alternate, as it can operate to 40V single supply.
Regards,
Yoworex
Hi
Thank you for your reply.
I close this question
best regards
N.Kokubo