Post Go back to editing

ADV3224 cascade connection query

Thread Summary

The user asked if two ADV3224 devices can be used to create a 32x8 switch matrix. The final answer confirms this is possible by using the daisy chain feature, as shown in the data sheet's Figure 65, which illustrates a 32x16 array using four ADV3224s. The engineer provided a diagram to support the configuration.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV3224

Hi:

   The datasheet of ADV3224 shows that ADV3224 support daisy chain ,Does it mean i can set up one 32*8 switch matrix by using two pcs ADV3224?

   Pls help check ,Thank you .