Hi:
The datasheet of ADV3224 shows that ADV3224 support daisy chain ,Does it mean i can set up one 32*8 switch matrix by using two pcs ADV3224?
Pls help check ,Thank you .
ADV3224
Production
The ADV3224/ADV3225 are high speed 16 × 8 analog crosspoint switch matrices. They offer a -3 dB signal bandwidth of greater than 750 MHz and a high slew...
Datasheet
ADV3224 on Analog.com
Hi:
The datasheet of ADV3224 shows that ADV3224 support daisy chain ,Does it mean i can set up one 32*8 switch matrix by using two pcs ADV3224?
Pls help check ,Thank you .
Hi,
The data sheet has a section titled Creating Larger Crosspoint Arrays on page 23 that addresses this issue. The example given in Figure 65 is to create a 32x16 array using four ADV3224s, however you could also create a 32x8 array by using only the two devices on the left in Figure 65.

Bruce
Hi,
The data sheet has a section titled Creating Larger Crosspoint Arrays on page 23 that addresses this issue. The example given in Figure 65 is to create a 32x16 array using four ADV3224s, however you could also create a 32x8 array by using only the two devices on the left in Figure 65.

Bruce