Hi:
The datasheet of ADV3224 shows that ADV3224 support daisy chain ,Does it mean i can set up one 32*8 switch matrix by using two pcs ADV3224?
Pls help check ,Thank you .
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADV3224
Production
The ADV3224/ADV3225 are high speed 16 × 8 analog crosspoint switch matrices. They offer a −3 dB signal bandwidth of greater than 750 MHz and a high...
Datasheet
ADV3224 on Analog.com
Hi:
The datasheet of ADV3224 shows that ADV3224 support daisy chain ,Does it mean i can set up one 32*8 switch matrix by using two pcs ADV3224?
Pls help check ,Thank you .
Thanks for your question. I have forwarded it to the relevant support engineer
Hi,
The data sheet has a section titled Creating Larger Crosspoint Arrays on page 23 that addresses this issue. The example given in Figure 65 is to create a 32x16 array using four ADV3224s, however you could also create a 32x8 array by using only the two devices on the left in Figure 65.

Bruce