is there any pin equivalent of ADG439F,SO16 package , fault protected
ADG439F
Production
The ADG438F and ADG439F are CMOS analog multiplexers, with the ADG438F comprising eight single channels and the ADG439F comprising four differential channels...
Datasheet
ADG439F on Analog.com
is there any pin equivalent of ADG439F,SO16 package , fault protected
Hello,
The ADG509F is a similar device, that would be pin for pin compatible in a SOIC package. The ADG509F is only specified up to 85C and some of the parameters are different so the ADG439F, most notably leakage.
The ADG5209F is an upgraded version of the ADG439F but unfortunately it is only available in TSSOP or LFCSP packages.
The only other pin for pin device would be the ADG409, however the ADG409 does not include integrated fault protection.
Regards,
David
Hello,
The ADG509F is a similar device, that would be pin for pin compatible in a SOIC package. The ADG509F is only specified up to 85C and some of the parameters are different so the ADG439F, most notably leakage.
The ADG5209F is an upgraded version of the ADG439F but unfortunately it is only available in TSSOP or LFCSP packages.
The only other pin for pin device would be the ADG409, however the ADG409 does not include integrated fault protection.
Regards,
David