Post Go back to editing

ADG439F

Category: Hardware

is there any pin equivalent of ADG439F,SO16 package , fault protected 

Top Replies

  • Hello,

    The ADG509F is a similar device, that would be pin for pin compatible in a SOIC package. The ADG509F is only specified up to 85C and some of the parameters are different so the ADG439F, most notably…

  • Hello,

    The ADG509F is a similar device, that would be pin for pin compatible in a SOIC package. The ADG509F is only specified up to 85C and some of the parameters are different so the ADG439F, most notably leakage.

    The ADG5209F is an upgraded version of the ADG439F but unfortunately it is only available in TSSOP or LFCSP packages.

    The only other pin for pin device would be the ADG409, however the ADG409 does not include integrated fault protection.

    Regards,

    David