Post Go back to editing

ADG812 NC pin 4 and 12

It looks like I can use the ADG812 as an alternate part for the ADG5412 but I want to confirm that I can ground the pin-4 (NC) as well as pull up pin-12 (NC) to 3.3V via 100K.  I realize I will lose the Fault Detection feature but if I can leave that pin pulled high at least I will not have false faults detected by my FPGA.

-Nate