Post Go back to editing

About the power supply voltage of ADG734

Thread Summary

The user inquired about using the ADG734 with a ±3.3V power supply. The final answer confirmed that while the part can operate within the Absolute Max Ratings (7V swing), performance is not guaranteed and using ±3.3V is not recommended. Additional clarification noted that the part is tested and guaranteed only at ±2.5V.
AI Generated Content

Hello


I have a question about the power supply voltage of the ADG734.
In the Features of P1 of the data sheet, it is stated that dual power supplies are ± 2.5V.
Also, regarding the characteristics, there is only ± 2.5V data of P4.
Can this device be used at ± 3.3V?
It seems that the rating has not been exceeded.

Best Regards,
Knj