Post Go back to editing

ADG1408: What leads to the high noise contribution with this analog multiplexer?

Thread Summary

The user observed a 20x higher noise in a programmable gain stage using the ADG1408 multiplexer compared to a fixed gain stage. The final answer suggests that the simulation model may not be optimized for noise performance, and the reference voltage source used in the simulation does not significantly affect the noise analysis. The user should ensure the switch is closed during the noise simulation to accurately assess performance.
AI Generated Content

Hi, I am new to this board and I am still trying to find my way around.

Here's my question:

For audio processing purposes, I would like to use a programmable gain stage based on the 8:1 multiplexer ADG1408 and get a qualitative feel for the performance by comparing it against a fixed gain stage. When I look at the time domain, I see pretty good correspondence between the two gain stages. However, when I compare the noise performance, I see a 20x higher noise with the programmable gain stage. Is this really to be expected? Why is it so high? I've added the asc file add the bottom of this post..

6840.mwe2.asc

Edit Notes

Fixed typo
[edited by: Kepa at 8:48 PM (GMT -5) on 13 Dec 2021]
Parents
  • Hi,

    Thanks for your patience.

    I like to ask why you are analyzing the noise of the mux_gain output to the digital EN logic, V1 input of the ADG1408?

    I have tried simulating the noise of the mux_gain of the amplifier with the ADG1408 connected and disconnected w.r.t. the V9 input and, I don't see any significant difference.

    Best regards,
    Christian

  • My apologies for the late reply. The notification from ADI went in my spam folder and since I moved on to the LTC6912, I didn't have the need to monitor this thread.

    In any case: does it really matter which voltage source I use as a reference? I have switched from V1 to V9 but see no difference. The noise hovers at around 14 µV/sqrt(Hz) when the mux is used, whereas the reg_mux node shows only about 700 nV/sqrt(Hz).

  • Hi,

    It shouldn't matter whatever voltage source you use as a reference in noise analysis. It seems that the simulation model is not optimized for noise performance simulation.

    Best regards,
    Christian

Reply Children
No Data