Post Go back to editing

ADG708 Power sequence

Thread Summary

The user asked if it's safe to tie the ENABLE pin of the ADG708 multiplexer to the 3V supply to permanently enable the device. The engineer confirmed that tying the ENABLE pin high will keep the multiplexer enabled, and the circuit should work correctly as long as the 500mVpp sine wave with a 1.13V DC bias is within the device's performance max ratings.
AI Generated Content

In terms of power sequencing for the ADG708 mux  is it OK to tie the ENABLE pin permanently to a system GND to permanently enable the multiplexer?
This means the enable input will be tied low as power is applied and I do not want to risk damage or stress to the CMOS etc
The multiplexer is used in a single supply 3V system
Many thanks for any info

Parents Reply
  • Hi Elver,

    Would you be able to provide an image or a block diagram of your application.

    If Enable is tied high depending on the inputs to the Analog input channels any number of switch channels could be ON.

    To answer your question on risk of damage, the least risk of damage will be when the switch is OFF or when the switch is ON and within the Performance / Max Rating of the device.

    Will need more information here to fully answer this questions, please provide block diagram / circuit image.

    Regards,

    Kevin

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.