Post Go back to editing

ADG5206 minimum voltage requirements

Thread Summary

The user inquired if the ADG5206 can operate with VDD = +3.3V and VSS = -3.3V. The final answer confirmed that the ADG5206 operates within +/-9V to +/-22V, making +/-3.3V unsuitable. The ADG1606 was suggested as an alternative, but the user noted it has too high charge injection. The support engineer then recommended the ADG658 or ADG608 for lower charge injection, though no data is provided for +/-3.3V operation.
AI Generated Content

Hello!

Does the ADG5206 work with VDD = +3.3V and VSS = -3.3V?

Im trying to subsitute ADG1206 with ADG5206 and want to know if I can power it with the stated VDD and VSS values. I have been studying datasheet for both muxes but cannot find if ADG5206 can be powered and used with +/-3.3V.

Datasheet ADG5206

Thanks