ADG5412
Recommended for New Designs
The ADG5412/ADG5413 contain four independent single-pole/single-throw (SPST) switches. The ADG5412 switches turn on
with Logic 1. The ADG5413 has two switches...
Datasheet
ADG5412 on Analog.com
ADG5412F
Recommended for New Designs
The ADG5412F and ADG5413F contain four independently controlled single-pole/single-throw (SPST) switches. The ADG5412F has four switches that turn on with...
Datasheet
ADG5412F on Analog.com
Hi!
I am using ADG5412F on my project, but, due to the shortage, I must change it with something else.
I see there are many ADG5412 products: ADG5412, 5412F, 5412F-EP, 5412W. But I cannot find an easy way to compare them all in order to know which of them could be suitable for my project.
Does anyone know of a comparison table or so?
Thanks in advance.
Stefano
Hi Stefano,
If you require the fault protection of the ADG5412F, I would suggest the next best alternative is the ADG5412BF. The BF version has fault protection on both the S and D sides of the switch.
If fault protection is not critical for your application you could look at the ADG5412 or the ADG1412.
The EP version of the ADG5412F is an enhanced product with more specifications including specifications for -55C
The W version of the ADG5412 is an automotive qualified version of the device.
Regards,
David
Hi Stefano,
If you require the fault protection of the ADG5412F, I would suggest the next best alternative is the ADG5412BF. The BF version has fault protection on both the S and D sides of the switch.
If fault protection is not critical for your application you could look at the ADG5412 or the ADG1412.
The EP version of the ADG5412F is an enhanced product with more specifications including specifications for -55C
The W version of the ADG5412 is an automotive qualified version of the device.
Regards,
David