Post Go back to editing

Requesting for suggestion of analog SPDT switch IC

Hello,

There is an requirement for Analog SPDT switch for our application board.

In the input port, either an analog AC video signal or GPIO signal is provided, depending on the input signal using an control pin need to direct the signal to output port as shown in attached image. 

Could you please suggest the below mentioned negative voltage supported SPDT IC part number for our application?

Requirement:

1. 1:2 single analog SPDT switch

2. Input should support AC signal type going from -300mV to 300mV and clocked at a 74.25MH

Thanking you in advance.