ADG3257

Is there any 2:1/ 4:1 Mux/Bus switch available for the below mentioned requirements.
Inputs range:
* Generating 1x16MHz at 5V logic and 1x16MHz at 3.3V logic and I want to select any one of the clock.
* Input voltage level: 3.3V and 5V
* Input Logic: LVCMOS and CMOS/TTL
Output requirements:
* Output: 5V(CMOS/TTL) or 3.3V (LVCMOS)
Please let me know whether ADG3257 part will be suitable for this requirement.
Thank you.

Top Replies

Parents
  • Thank you for your reply.

    I am going to provide two different logics at input side such as 5V and 3.3V logic and I need to take output at 5V logic.

    I need to level translate the input signals to 5V logic and I need to select anyone of the signal through the switch. So, I need a device which have to perform level translation and Mux selection.

Reply
  • Thank you for your reply.

    I am going to provide two different logics at input side such as 5V and 3.3V logic and I need to take output at 5V logic.

    I need to level translate the input signals to 5V logic and I need to select anyone of the signal through the switch. So, I need a device which have to perform level translation and Mux selection.

Children