Hi,
I used to micom connect ADG451 1,8,9,16(in)pins
but, After turning off the +15v/-15v power, my microcomputer started to heat up. What is the reason?
Do I need a switching circuit (TR/FET) on pins 1,8,9,16?

Thank you.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
ADG451
Production
The ADG451 is a monolithic CMOS device comprising four independently selectable switches. It is designed on an enhanced LC2MOS process which provides low...
Datasheet
ADG451 on Analog.com
Hi,
I used to micom connect ADG451 1,8,9,16(in)pins
but, After turning off the +15v/-15v power, my microcomputer started to heat up. What is the reason?
Do I need a switching circuit (TR/FET) on pins 1,8,9,16?

Thank you.
Hi,
The ADG451 IN pins have internal esd protection diodes. it is likely that you have violated the max ratings of the ADG451.
The digital inputs must be kept with in 2 volts of the supply.
To prevent this you could consider our overvoltage protection switches such as the ADG5412F.
These devices can stand off voltages up to 48 V on the digital pins, both in the power on and power off condition.
Thanks
David