Post Go back to editing

Confusion regarding peak power and continuous power consumption for ADG1404

Thread Summary

The user observed a peak current of 68 mA during a transient response when switching the control input of the ADG1436 analog mux, leading to a high power dissipation of 2.04 W. The support engineer clarified that this is a short-lived transient (3 ns) and the continuous current per channel for both ADG1404 and ADG1436 is up to 400 mA, with the operating power consumption being much lower at 10.79 mW in the worst case.
AI Generated Content

I am using the mux using ±15V of supply. I'll be passing signals with voltages between ±3V through the analog mux and a max (passthrough) current of 50mA. I'll be using +15V for 'enable' input (always 'ON') and +3.3V for mux control input. Now looking at the datasheet the max current Idd is 285uA and the max current Iss is 1uA. So the operating power consumption should be equal to 15V*285uA + 15V*1uA=4.29mW. 

Now at  ±15V, the max Ron is 2.6 so the power dissipation for a current of 50mA is (50mA)^2 * 2.6 = 6.5mW. So the total worst-case power consumption (please correct me if my calculations are wrong) should be  6.5+4.29=10.79mW

But now when I try to simulate a similar (in terms of capacitance, resistance, and power requirements) model ADG1436 (since ADG1404 is not available): 



I see that when the control input changes from low to high (0->3.3), there is a peak current of around 68mA at +15V (green, I(V3)) line and -68mA at -15V (red, I(V2)) line. So total power would be 15V*68mA+15V*68mA =2.04W. Which seems way too much for a switch. Could someone clarify the continuous power and peak power consumption for ADG1404?

Thank you.

Edit Notes

spelling
[edited by: paulplusx at 10:50 PM (GMT -4) on 19 Mar 2021]
Parents
  • Hi Paul,

    Upon looking into this, the current of around +/-68 mA is a transient response that only lasts for about 3 ns. We haven't modeled these Idd/Iss parameters yet. May we know your application, and is the power consumption is your top priority in your design and simulations?

    Both the ADG1404 and ADG1436 have a continuous current per channel rating of up to 400 mA.

    Best regards,
    Christian

Reply
  • Hi Paul,

    Upon looking into this, the current of around +/-68 mA is a transient response that only lasts for about 3 ns. We haven't modeled these Idd/Iss parameters yet. May we know your application, and is the power consumption is your top priority in your design and simulations?

    Both the ADG1404 and ADG1436 have a continuous current per channel rating of up to 400 mA.

    Best regards,
    Christian

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.