ADG3123 analog voltage range

To whom it may concern, 

I am intrigued by the ADG3123 because it affords logic-level to high-voltage bipolar outputs. However, I do not necessarily need the high voltage range specified in the part datasheet. Can this part operate at VDDA=VDDB=3V or VDDA=VDDB=5V and VSS=0V levels? This is a typical use case for my application. 

While the datasheet describes the min recommended VDDB to GND and VDDB to VSS is 10.8V, I believe my above biasing conditions do not violate the absolute max ratings (i.e. VDDA <= VDDB, as well as what is shown in the screen capture below).

Please advise.

Thank you kindly,

Scott 

Parents Reply Children
No Data