Post Go back to editing

ADG5419 with Enable in MSOP package?

Hi,

The ADG5419 has a nice enable feature but only in the LFCSP package (kind of a DFN package).

In the MSOP package, the enable seems to be just not bonded from the chip to the lead frame.

This is very unfortunate, as this enable feature is really advantageous, but the LFCSP package cannot be used in applications which do not tolerate the lower reliability versus temperature cycling of the no-lead packages.

I understand that there are reasons for leaving pin 5 unconnected for compatibility issues with existing switches, but just not offering the feature in the MSOP package seems not to be the brightest idea.
Also having the same part number but different functionality in different packages is quite confusing.

Is there a comparable part that has both, the enable feature and a gull wing package?
Or could ADI make available a version of the ADG5419 that has enable bonded to pin 5 of the MSOP package? There would be virtually no additional production cost as one additional wire bond should be negligible. Of course there is also cost associated with introducing a "new" part and maintaining it, but there would also be additional revenue.

Best Regards,
Gerd

  • Hi Gerd,

    Unfortunately we do not have a SPDT device in a MSOP package with an enable pin. 

    As you have said, this is to maintain compatibility with legacy devices.

    At the moment there are no plans to release an MSOP version with an enable pin but your feedback is greatly appreciated and will be considered in future developments.

    Regards,

    Stephen

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.