Post Go back to editing

ADG419 Application

Hello,

Can i give both negative dc signal at  S1 and S2 of the switch and switch between them using control signal?

Regards..

Parents
  • Hi, Naidu.

    As long as your signals at S1 and S2 are within Vss to Vdd signal range, you should have no problem using the ADG419. Just bear in mind that you will need to power up the ADG419 with dual supplies (greater than +/-5 V, as we cannot guarantee normal operation with lower supplies), and that this part is specified with VL = 5 V, and VIN = 5 V.

    Yours sincerely,

    Igor Ono.

Reply
  • Hi, Naidu.

    As long as your signals at S1 and S2 are within Vss to Vdd signal range, you should have no problem using the ADG419. Just bear in mind that you will need to power up the ADG419 with dual supplies (greater than +/-5 V, as we cannot guarantee normal operation with lower supplies), and that this part is specified with VL = 5 V, and VIN = 5 V.

    Yours sincerely,

    Igor Ono.

Children