Hello,
Can i give both negative dc signal at S1 and S2 of the switch and switch between them using control signal?
Regards..
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
ADG419
Production
The ADG419 is a monolithic CMOS SPDT switch. This switch is designed on an enhanced LC2MOS process that provides low power dissipation yet gives high switching...
Datasheet
ADG419 on Analog.com
Hello,
Can i give both negative dc signal at S1 and S2 of the switch and switch between them using control signal?
Regards..
Hi, Naidu.
As long as your signals at S1 and S2 are within Vss to Vdd signal range, you should have no problem using the ADG419. Just bear in mind that you will need to power up the ADG419 with dual supplies (greater than +/-5 V, as we cannot guarantee normal operation with lower supplies), and that this part is specified with VL = 5 V, and VIN = 5 V.
Yours sincerely,
Igor Ono.
Thanks Ono,
My power supplies are +/- 12V and S1 and S2 are 12V and -12V
VL=5V and VIN =3.3V.
Are the above supplies ok?
Regards..
Hi, Naidu.
Your supply voltages and voltages at S1 and S2 are within datasheet limits, so your device should work as expected.
Yours sincerely,
Igor Ono.