Post Go back to editing

We have an ADV3229 eval board and the software is running on a computer with Win XP OS. It does not appear to be recognized by the computer. We get no errors when pressing the radial buttons. We get no errors even with the USB disconnected.

Hi,

We have an ADV3229 eval board and the software is running on a computer with Win XP OS.  It does not appear to be recognized by the computer.  We get no errors when pressing the radial buttons.  We get no errors even with the USB disconnected.

Please help...

Don

Parents
  • Hey Goz,

    The board powers up and the USB LED it lit.  When I send the load script (all 8 outputs on), the D1 and D2 LEDs toggle back and forth.  There is no outputs on any parallel or serial breakout pins.  Can the LEDs toggle if the firmware is not loaded in the USB IC?  Is the firmware loaded at the factory or downloaded by the GUI?

    Don

Reply
  • Hey Goz,

    The board powers up and the USB LED it lit.  When I send the load script (all 8 outputs on), the D1 and D2 LEDs toggle back and forth.  There is no outputs on any parallel or serial breakout pins.  Can the LEDs toggle if the firmware is not loaded in the USB IC?  Is the firmware loaded at the factory or downloaded by the GUI?

    Don

Children
No Data